Heat and dust: energy supply system for indoor crane under adverse conditions

Profile

  • What was needed: Pre-assembled energy chain for use in a heavy-duty application
  • Requirements: Tight installation space, resistance to high temperatures and heavy soiling, trouble-free operation
  • Area of application: Steel industry
  • Success for the customer: Quick assembly on the crane bridge by delivering the filled energy chain on transport drums. The very compact chains also do not have to be dismantled or packed for onward transport to the place of use.
Portal industrial galben mare cu mai multe poduri rulante într-o hală.

Problem

Solution

The crane is constantly exposed to high levels of dust and high temperatures. The slabs and the hot holding furnace emit so much heat that temperatures up to 70 degrees Celsius are reached even just below the ceiling of the hall.

Dipl. Ing. Mike Götzensberger

Project manager at Bang

Sistem de lanț portcablu într-o instalație industrială ghidează cablurile și furtunurile de-a lungul traseului.
Lanț portcablu pe un utilaj industrial galben.

Consultanta

Mi-ar face placere sa va raspund personal la întrebari

Expediere și consultanță