Pod arcuit noaptea, cu structură de oțel iluminată pe fundalul cerului întunecat.

The world's largest polymer energy chain

Many times lighter than comparable steel chains, it effortlessly moves more than 100 kg of filling weight per metre

Profile

  • What was needed: energy chain E4.350 from the E4.1. series, aluminium guide trough with floating moving end, i.Sense Condition Monitoring System
  • Requirements: Long minimum service life of 15 years without major maintenance, continuous operation 365 days a year
  • Industry: Sludge dewatering
  • Success for the customer: Close collaboration in the engineering process and creation of a customised solution, extensive laboratory tests to check the suitability of the system for the application, on-time installation of a compact and lightweight energy supply system, low maintenance and failure-free to date

Problem

Solution

We were impressed by the fact that the entire energy chain system is very compact. On the other hand, the plastic chain is much lighter compared to a steel chain. You need lesser forces to pull them from one end of the bridge to the other.

Joury van Gijseghem

Project manager DEME

Stație de tratare a apei cu bazine rotunde și canale, văzută de sus.
Pod transportor pe un șantier, cu lanț portcablu și componente de mașină.

Convincing project competence

Un lanț portcablu negru traversează un pod sau pasaj, lângă o zonă industrială.

Consultanta

Mi-ar face placere sa va raspund personal la întrebari

Expediere și consultanță