Cost savings for airport operators

iglidur® bearings defy aggressive conditions in various airport applications

Profile

  • What was needed: iglidur®plain bearing
  • Requirements: Bearings were needed that are used continuously outdoors, in extreme cold and heat as well as under the influence of acidic de-icing agents. The materials must also not absorb water, which would otherwise freeze.
  • Industry: Aerospace, airport
  • Success for the customer: The iglidur® bearings are light, robust, weatherproof and lubrication-free, which means they can be used in extreme cold. In the iglidur® Z version, they are even certified for temperatures as low as -100 °C. The extensive range helps the customer to obtain solutions for all requirements from a single source.
Furtun galben flexibil cu racord metalic pentru Bearings într-o aplicație Quickloading.

Problem

Solution

"The iglidur product range was just right for us. Lightweight, robust, weatherproof and lubrication-free, these were our most important points, certified in the iglidur Z version down to -100°C - that was the end of our search.

Armin Van der Lelij

CEO of the Quickloading development office

Rulmenți într-un dispozitiv Quickloading cu două bile de prindere.
Un deget indică o fixare de rulment cu șurub și suport metalic.

Further practical examples convince airport operators

Sistem de rulmenți Quickloading cu două elemente de ghidare cilindrice și pârghie.
Rulment cu componentă Quickloading pe un cărucior de transport în aer liber, ghidat de o persoană.

Consultanta

Mi-ar face placere sa va raspund personal la întrebari

Expediere și consultanță