Modificarea limbii :

Winner of the golden vector awards 2024: How did galaxies form? Where do exoplanets with life-friendly conditions exist? A multi-object and near-infrared spectrograph from MOONS Consortium, which also includes the Institute of Astrophysics and Space Sciences, is set to provide answers. The engineers rely on energy chains from the triflex® series from igus® for the precise and interference-free movement of the sensitive optical fibres. For the jury of the vector award 2024, the most spectacular e-chain® application.
În persoana:
Luni - Vineri de la 7 am la 8 pm.
Sâmbata de la 8 am la 12 pm.
Online:
24h